This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432 Custom Bootloader



Is there any example code available for a custom bootloader for the MSP432?

I am looking for the code that prepares the micro and then jumps to the main program (say, defined at 0x8000).

I assume you need to set the interrupt vector table location and jump to the new start location? How is this best achieved?

  • Hi Josh,

     I have been working on a similar example code.

    Josh Adler2 said:
    I assume you need to set the interrupt vector table location and jump to the new start location? How is this best achieved?

    Yes that is correct and I do not have any problem sharing these projects, but before doing that, which IDE (CCS/IAR/KEIL) are you using??

      Regards,

       David

  • Hi David,

    I am using CCS 6.1. I tried to click on the image, but I get access denied.

    Regards,

    Josh
  • Hi Josh,

    I just updated the image. I'll try to have the example projects by tomorrow.

    Thanks,

    David
  • Thanks David.

    I think I have it sorted, I have my cmd files with App1 at 0x0000 and App2 at 0x8000,

    then in App1's CMD file:

    --retain=interruptVectors
    --retain=flashMailbox
    
    MEMORY
    {
        FLASH_BOOT (RX) : origin = 0x00000000, length = 0x00008000
        FLASH     (RX) : origin = 0x00008000, length = 0x00038000
        FLASH_OTP (RX) : origin = 0x00200000, length = 0x00004000
        SRAM      (RWX): origin = 0x20000000, length = 0x00010000
    }
    
    /* The following command line options are set as part of the CCS project.    */
    /* If you are building using the command line, or for some reason want to    */
    /* define them here, you can uncomment and modify these lines as needed.     */
    /* If you are using CCS for building, it is probably better to make any such */
    /* modifications in your CCS project and leave this file alone.              */
    /*                                                                           */
    /* --heap_size=0                                                             */
    /* --stack_size=512                                                          */
    /* --library=rtsv7M4_T_le_eabi.lib                                           */
    
    /* Section allocation in memory */
    
    SECTIONS
    {
        .intvecs:   > 0x00000000
        .text   :   > FLASH_BOOT
        .const  :   > FLASH_BOOT
        .cinit  :   > FLASH_BOOT
        .pinit  :   > FLASH_BOOT
    
        .flashMailbox : > 0x00202000
    
        .vtable :   > 0x20000000
        .data   :   > SRAM
        .bss    :   > SRAM
        .sysmem :   > SRAM
        .stack  :   > SRAM (HIGH)
        //.stack  :   > SRAM (HIGH), fill = 0xCDCDCDCD
    }
    

      

     And App1's code:

    {

      SCB->VTOR = 0x8000;
    
      //
      // Load the stack pointer from the application's vector table.
      //
      __asm("    ldr     r1, [r0, #0]\n"
          "    mov     sp, r1\n");
    
      //
      // Load the initial PC from the application's vector table and branch to
      // the application's entry point.
      //
      __asm("    ldr     r0, [r0, #4]\n"
          "    blx      r0\n");

    App2's CMD File

    --retain=interruptVectors
    --retain=flashMailbox
    
    MEMORY
    {
        FLASH_BOOT (RX) : origin = 0x00000000, length = 0x00008000
        FLASH     (RX) : origin = 0x00008000, length = 0x00038000
        FLASH_OTP (RX) : origin = 0x00200000, length = 0x00004000
        SRAM      (RWX): origin = 0x20000000, length = 0x00010000
    }
    
    /* The following command line options are set as part of the CCS project.    */
    /* If you are building using the command line, or for some reason want to    */
    /* define them here, you can uncomment and modify these lines as needed.     */
    /* If you are using CCS for building, it is probably better to make any such */
    /* modifications in your CCS project and leave this file alone.              */
    /*                                                                           */
    /* --heap_size=0                                                             */
    /* --stack_size=512                                                          */
    /* --library=rtsv7M4_T_le_eabi.lib                                           */
    
    /* Section allocation in memory */
    
    SECTIONS
    {
        .intvecs:   > 0x00008000
        .text   :   > FLASH
        .const  :   > FLASH
        .cinit  :   > FLASH
        .pinit  :   > FLASH
    
        .flashMailbox : > 0x00202000
    
        .vtable :   > 0x20000000
        .data   :   > SRAM
        .bss    :   > SRAM
        .sysmem :   > SRAM
        .stack  :   > SRAM (HIGH)
        //.stack  :   > SRAM (HIGH), fill = 0xCDCDCDCD
    }

    Anything missing? Seems to work as expected, just not sure about the loading of the VTOR register.

    Regards,

    Josh

  • Hi Josh,

     That's exactly how I did it. The only difference is that for VTOR, I used the "interruptVectors" (msp432_startup_ccs.c) instead of the address. Something like this:

    SCB->VTOR = (uint32_t)interruptVectors;

    Hopefully this helps.

      David 

  • Hi David,

    Won't that be the interruptVectors for the current application (bootloader) instead of the application you are calling (main code)?

    /* Interrupt vector table.  Note that the proper constructs must be placed on this to */
    /* ensure that it ends up at physical address 0x0000.0000 or at the start of          */
    /* the program if located at a start address other than 0.                            */
    #pragma RETAIN(interruptVectors)
    #pragma DATA_SECTION(interruptVectors, ".intvecs")
    void (* const interruptVectors[])(void) =
    {
        (void (*)(void))((uint32_t)&__STACK_END),
                                                /* The initial stack pointer */
        resetISR,                               /* The reset handler         */
    ...
    ...
        defaultISR                              /* Reserved 63               */
    };
    

    Josh

  • Hi Josh,

    I believe it should depend on who (application or boot loader) is writing to the SCB->VTOR register. In my case the boot loader passes the control to the application who actually writes to the SCB->VTOR register.

    Hopefully this helps.

    David
  • Hi David,

    That sounds sensible, but I do it in the bootloader in order to determine the reset vector address so the bootloader knows where to jump. How do you do that part without setting VTOR?

      SCB->VTOR = 0x8000;
    
      //
      // Load the stack pointer from the application's vector table.
      //
      __asm("    ldr     r1, [r0, #0]\n"
          "    mov     sp, r1\n");
    
      //
      // Load the initial PC from the application's vector table and branch to
      // the application's entry point.
      //
      __asm("    ldr     r0, [r0, #4]\n"
          "    blx      r0\n");
    

**Attention** This is a public forum