This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello!
I have two boards with CC430F5137. When I try to connect to board by JTAG (MSP430-FET430UIF, v1.4a), I get error ("Fatal error: Could not find device (or device not supported) Session aborted!" ). This error occure when I use 4-wired JTAG and spi-bi-wire. For programming I use IAR MSP IDE v6.5.0.
**Attention** This is a public forum