This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does MSP430Ware Driver Library work on MSP430F169

Other Parts Discussed in Thread: MSP430F169, MSP430WARE

Hi, 

I am using Code Composer and have been trying to import the Driver Library of MSP430ware to a project based on MSP430F169 but it doesn't seem to work. 

The resource explorer of MSP430ware on CCS shows that the Driver Library is available for the following micro families MSP430FR57xx , MSP430FR5xx_6xx, MSP450FR3xx_4xx and MSP430i2xx, does this mean that it does not work on MSP430F169.

For this particular project i have to use MSP430F169, and i also would like to take advantage of the Driver library to write a well layered and structured program rather than having to deal with low level particulars (register level code) which i can do if there are no other options, 

any help is highly appreciated. 

Thanks 

NK

 

**Attention** This is a public forum