Hello ,
I'm using MSP430F5131 micro-controller .
I'm using an external oscillator of 12.8MHz which connected to pins PJ.4 and PJ.5 and defined P2.4 ( with timer : TD0.0) as my 1 pulse per second output.
I would like to generate a 1 pulse per second using this external oscillator through P2.4 . In addition to this 1 PPS i got a toggle switch that toggles between a "normal" 1 pulse per second and a "bad" pulse of 0.5 second.
First of all i would like to know how to write a proper code of 1PPS and then i would like to implement both of the pulses ("normal" and "bad") into the code.
I have written a code of a 1PPS , i'm not sure if i have written it correctly :
TD0CCR0=49999; // setting TAR count up value -1
TD0CCTL0=CCIE; //enabling interuption
TD0CTL0 =MC_1|ID_3|IDEX_3|TDSSEL_0|TDCLR; //defining timer d TD0.0 (P2.4)
__enable _interrupt ();
for(;;){
if ((P1IN & BIT2)==0) { //ACTIVE LOW
#pragma vector = TIMERD0_VECTOR //GENERATES 1PPS EVERY 1s
__interrupt void TD0_ISR (void){
P2OUT ^=BIT4;//TOGGLE THE 1PPS PULSE ('1' - '0' )
}
}
}
Thanks in advance.