This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: Problem with adding driver library (drivelib) to the existing project: stuck at the Reset_Handler

Part Number: MSP432P401R


I recently completed RTOS course based on MSP432 Red Launchpad. I also came across the driver library (drivelib) for the MSP432 launchpad and I wanted to use it in my existing projects. But whenever I include any driver library functions to my existing project, the code does not run. When I tried to debug, the control is stuck at the Reset_Handler of the startup_msp432p401r_uvision.sfile. Whenever I comment out the driver library functions such as  MAP_WDT_A_holdTimer(), the code runs fine. Here's my main function:

int main(void){
		OS_Init();
		UART0_Init();
		OutValue("\n\rPWM Dutycycle =",0);
			
		/* Halting the watchdog */
//		 MAP_WDT_A_holdTimer();
	        /* Configuring GPIO2.4 | GPIO2.5 as peripheral output for PWM  and P1.4 | P1.1 for button
                * interrupt */
//              MAP_GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P2, GPIO_PIN4,
//              GPIO_PRIMARY_MODULE_FUNCTION);
						
//		P2SEL0 |= 0x10;
//		P1SEL1 &= ~0x10;                      // configure P2.4 as primary module function				
						
//		/* Configuring Timer_A to have a period of approximately 500ms and
//              * an initial duty cycle of 10% of that (3200 ticks)  */
//              MAP_Timer_A_generatePWM(TIMER_A0_BASE, &pwmConfig1);

                return 0;           
}






Whenever I uncomment any MAP_ functions which are the driver library functions, the code gets stuck:

I have also attached my project folder if anyone wants to try out.6433.Timer_A_with_Lab6.zip

  • Hello,

    Thank you for your interest in our product!  I am looking into this issue for you and I expect I will have a response for you by tomorrow.

  • Hello,

    I know I promised a response today, so I'll give you an update.  I notice it appears you are using KEIL IDE.  I use CCS.  I began looking into this this afternoon and ran into a lot of include/library types of errors which I had to workout before I could even build the project properly.  I did get it built so that it is ready to run and I can start looking into the debug of the issue you are having now, but I am out of time for today.  Tomorrow I will continue by loading your code onto my launchpad device and then running through debug to replicate and then resolve your issue.

    Thank you for your patience.

  • Thanks John for the update. Looking forward.

  • I was not able to replicate the issue yet because I am runnning into a different issue with loader_exit() occuring.

    I am curious what RTOS is this as it does not look like it is TI_RTOS.  Are you using TI_RTOS or another RTOS?

    Also, I have asked around a little bit and a common concern I have heard is if the watchdog timer is being turned off in OS_init() here or if not whether the program is being halted due to the WDT prior to reaching the command to turn it off?  Have you tried moving the MAP_WDT_A_holdTimer() function above your OS_Init() ?

  • Hi John,

    The RTOS running is not TI_RTOS. I took Real-time Bluetooth Networks course and the project is based on that. It is not a full-fledged RTOS and not advanced like TI_RTOS or FreeRTOS. 

    John P. Morrison said:
    Have you tried moving the MAP_WDT_A_holdTimer() function above your OS_Init() ?

    Yes. I tried that also. But no effect. Even tried commenting MAP_WDT_A_holdTimer()  and adding only MAP_GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P2, GPIO_PIN4, GPIO_PRIMARY_MODULE_FUNCTION); 

    But same result. Stuck at the Reset_Handler.

     

  • Hello,

    I am wondering if you have been able to find a solution to this yet?  I was able to run a driverlib api inside of an TI-RTOS example today just by inserting the following:

    /* DriverLib Includes */

    #include <ti/devices/msp432p4xx/driverlib/driverlib.h>

    I started out using the empty TI-RTOS example.  Here is what I put into the empty.c file:

    /*
     * Copyright (c) 2015-2016, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    
    /*
     *  ======== empty.c ========
     */
    
    /* DriverLib Includes */
    #include <ti/devices/msp432p4xx/driverlib/driverlib.h>
    
    #include <stdbool.h>
    
    /* For usleep() */
    #include <unistd.h>
    #include <stdint.h>
    #include <stddef.h>
    
    /* Driver Header files */
    #include <ti/drivers/GPIO.h>
    // #include <ti/drivers/I2C.h>
    // #include <ti/drivers/SDSPI.h>
    // #include <ti/drivers/SPI.h>
    // #include <ti/drivers/UART.h>
    // #include <ti/drivers/Watchdog.h>
    
    /* Board Header file */
    #include "Board.h"
    
    /*
     *  ======== mainThread ========
     */
    void *mainThread(void *arg0)
    {
        volatile uint32_t ii;
    
        /* Configuring P1.0 as output */
        MAP_GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN0);
    
        while (1)
        {
            /* Delay Loop */
            for(ii=0;ii<500000;ii++)
            {
            }
    
            MAP_GPIO_toggleOutputOnPin(GPIO_PORT_P1, GPIO_PIN0);
        }
    }
    

    This managed to blink the led for me, using driverlib API's.

    I assume the Stuck at Reset_Handler may have to do with some other portion of the code and not directly related to the addition of driverlib functions.

     

  • Hi John,

    To accomplish my end task with my existing RTOS code, I used direct registry access instead of drivelib and it worked well. 

    Good to know that drivelib is working fine with TI-RTOS. Will try out. :)

**Attention** This is a public forum