This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SIMPLELINK-MSP432-SDK: MSP432: MAP_Timer_A_generatePWM function call generates only one pulse wave instead of true PWM wave

Part Number: SIMPLELINK-MSP432-SDK

Hello,

I'm using a Launchpad MSP432P401 with a BoosterPack MK-II.

I want to generate a PWM wave using MAP_Timer_A_generatePWM. I tried different samples coming from simplelink_msp432_sdk_1_30_00_40 SDK (timer_a_pwm_mode_MSP_EXP432P401R, nortos) and msp432_driverlib_3_21_00_05 SDK (timer_a_pwm_mode). I also try to use samples from the following e2e threads "e2e.ti.com/.../1531341" and from "https://e2e.ti.com/support/microcontrollers/msp430/f/166/t/427197".

Unfortunately, my issue is always the same : I just got one pulse, not a complete PWM wave. I used the following settings:

Timer_A_PWMConfig pwmConfig =
{
        TIMER_A_CLOCKSOURCE_SMCLK,
        TIMER_A_CLOCKSOURCE_DIVIDER_1,
        32000,
        TIMER_A_CAPTURECOMPARE_REGISTER_1,
        TIMER_A_OUTPUTMODE_RESET_SET,
        3200
};

Note that using TIMER_A in counter mode on the same GPIO and I got a nice PWM.

Do you have any idea to solve my issue?

Many thanks in advance for your support,

Best Regards,

Yann Garcia

  • Please show the complete program.
  • Hello Clemmens,

    Ouos, my apologies. Here is simplest sample I tried to make running:

    /* DriverLib Includes */
    #include <ti/devices/msp432p4xx/driverlib/driverlib.h>
    
    /* Standard Includes */
    #include <stdint.h>
    
    #include <stdbool.h>
    
    /* Timer_A PWM Configuration Parameter */
    Timer_A_PWMConfig pwmConfig =
    {
            TIMER_A_CLOCKSOURCE_SMCLK,
            TIMER_A_CLOCKSOURCE_DIVIDER_1,
            32000,
            TIMER_A_CAPTURECOMPARE_REGISTER_1,
            TIMER_A_OUTPUTMODE_RESET_SET,
            3200
    };
    
    int main(void)
    {
        /* Halting the watchdog */
        MAP_WDT_A_holdTimer();
    
        /* Setting MCLK to REFO at 128Khz for LF mode
         * Setting SMCLK to 64Khz */
        MAP_CS_setReferenceOscillatorFrequency(CS_REFO_128KHZ);
        MAP_CS_initClockSignal(CS_MCLK, CS_REFOCLK_SELECT, CS_CLOCK_DIVIDER_1);
        MAP_CS_initClockSignal(CS_SMCLK, CS_REFOCLK_SELECT, CS_CLOCK_DIVIDER_2);
        MAP_PCM_setPowerState(PCM_AM_LF_VCORE0);
    
        /* Configuring GPIO2.5 as peripheral output for PWM  and P6.7 for button
         * interrupt */
        MAP_GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P2, GPIO_PIN5,
                GPIO_PRIMARY_MODULE_FUNCTION);
        MAP_GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P5, GPIO_PIN1);
        MAP_GPIO_clearInterruptFlag(GPIO_PORT_P5, GPIO_PIN1);
        MAP_GPIO_enableInterrupt(GPIO_PORT_P5, GPIO_PIN1);
    
        /* Configuring Timer_A to have a period of approximately 500ms and
         * an initial duty cycle of 10% of that (3200 ticks)  */
        MAP_Timer_A_generatePWM(TIMER_A0_BASE, &pwmConfig);
    
        /* Enabling interrupts and starting the watchdog timer */
        MAP_Interrupt_enableInterrupt(INT_PORT5);
        MAP_Interrupt_enableSleepOnIsrExit();
        MAP_Interrupt_enableMaster();
    
        /* Sleeping when not in use */
        while (1)
        {
            MAP_PCM_gotoLPM0();
        }
    }
    
    /* Port1 ISR - This ISR will progressively step up the duty cycle of the PWM
     * on a button press
     */
    void PORT5_IRQHandler(void)
    {
        uint32_t status = MAP_GPIO_getEnabledInterruptStatus(GPIO_PORT_P5);
        MAP_GPIO_clearInterruptFlag(GPIO_PORT_P5, status);
    
        if (status & GPIO_PIN1)
        {
            if(pwmConfig.dutyCycle == 28800)
                pwmConfig.dutyCycle = 3200;
            else
                pwmConfig.dutyCycle += 3200;
    
            MAP_Timer_A_generatePWM(TIMER_A0_BASE, &pwmConfig);
        }
    }
    

    Thanks a lot for your support,

    Best regards,

    Yann Garcia

  • This is the example program, with the button input pin changed.

    Does the original example work? (But in theory, the button should not change anything.)

    How are you executing it? In a debugger, or just letting it run?

    What do you mean with "counter mode"? The timer always counts.
  • Yes you're right, this is what I wanted to explain: all the examples based on MAP_Timer_A_generatePWM() I found do not work: I just got a unique pulse.
    On the other way, the examples with TIMER_A in up/down mode (and using the same GPIO I used in my code) generate a PWM wave without any problem.
    It seems that only MAP_Timer_A_generatePWM() function causes some troubles.

    Best Regards,

    Yann Garcia

**Attention** This is a public forum