This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello everyone.
I used to program the msp430g2553 launchpad in Code Composer studio but this time I need to use energia to connect 2 msp430 to each other with i2c, I programmed both msps with Code Composer studio (disconnecting the jumper between the green LED and pin p1.6 on both launchpads and connecting the p1.6 and p1.7 pins of the launchpads with 10k pull-up resistors) and everything works correctly. But when I program the launchpads with energia with the example programs master_reader and slave_sender, the sda and scl signals are held high and nothing more. I tried to connect the slave first and then the master and I also tried to connect the master first and the slave after, and I tried to use the p2.1 and p2.2 pins as the picture shows.Nothing works.
Please, I need help and thanks beforehand for all
**Attention** This is a public forum