Other Parts Discussed in Thread: MSP430F5309, ENERGYTRACE
Hi,
Since the MSP-FET430UIF is discontinued, I just switched to the MSP-FET and I have issues working with it. Actually, I ordered a couple of msp-fet for our new production test benches and can't make them work properly...
I did program and debug in CCS 6.1.3.00034 using the MSP-FET but it seems to be really unstable and does not always work. Strangely, it seems to be related to the unit I'm programming, but I know this is not issue since I can always program and debug them when I switch back to the MSP-FET430UIF.
Most of the time, I get the errors: "Load program error" and "Cannot Erase memory".
What are the differences between the MSP-FET and MSP-FET430UIF that can make one work and not the other? Any specific requirements?
As specified, I'm using CCS 6.1.3.00034. I also tried with MSPFlasher 3.11 and I'm having the same error.
Please help,
M.