This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-FET: Difference between MSP-FET430UIF and MSP-FET

Part Number: MSP-FET

MSP-FET intentionally cut off VCC_TOOL when it sees some VCC_TARGET because it thinks the target has its own power.

Doesn't the same happen with  MSP-FET430UIF as well ?

  • Hello,

    RAJA BALAJI KARTHIKEYAN57 said:
    MSP-FET intentionally cut off VCC_TOOL when it sees some VCC_TARGET because it thinks the target has its own power.

    Yes, that's correct. As Jace mentions in the thread linked above, this functionality makes sure the voltage logic levels match the targets when powered by the MSP-FET or an external power supply.

    RAJA BALAJI KARTHIKEYAN57 said:
    Doesn't the same happen with  MSP-FET430UIF as well ?

    It may, but I guess I'm wondering why this would be an issue. As discussed, this functionality ensures that the logic levels match between the debugger and target. When you use either debugger, you should only use either VCC_TOOL or VCC_TARGET.

    Regards,

    James

**Attention** This is a public forum