This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello everyone,
as i have look in the example of MSP430G2955 examples code,atasheet and user's example, i don't find the way to shift the 7-bit I2C slaveaddress to the left and add the R/W bit? i am bit confused.which regiter i should use and bit? is it UCTR bit that represent the R/W bit,is it the UCB0I2CSA where i have to use the left shiftin?
thanks
**Attention** This is a public forum