Hi All,
Please tell me about TLV Data of MSP430FR5847.
It is stated in Table 5-30 (2) on page 48 of the data sheet(slase34d) as 30℃ ± 3℃ and 85℃ ± 3℃.
Customer converts the built-in temperature sensor using 1.2 V built-in reference, then reads TLV Data and calculates it.
(It is calculated from Address 0x1A1A (30℃) and 0x1A1C (85℃))
When 200 prototypes were trial-produced, it was almost good, but two items with a large error (5 - 6 ° C) were found.
When comparing the TLV of the two and the other MCU, it is that it is greatly different.
Then please tell me the following contents.
1. Is this accuracy of ± 3℃ guaranteed?
2. Please tell me the extent to which the calibration value of the temperature sensor fluctuates.
3. Is there a possibility that the calibration data varies greatly?
Best Regards,
Takashi