Hi,
We have problem with programming an unprogrammed MSP430F5510 through
"Firmware Upgrade Example" GUI tool + customer Board.
Every time when we press the "Upgrade Firmware" button it tries to
program the MSP but always gets unplugged as shown below.
The program used is GUI's Blink sample code.
Starting
Password Sent Successfully
Sending RAM BSL v00.07.08.38
Done RAM BSL v00.07.08.38
USB device was unplugged!
Unsuccessful in starting the BSL. Restarting.
Password Sent Successfully
Sending RAM BSL v00.07.08.38
Done RAM BSL v00.07.08.38
USB device was unplugged!
What could be the possible reason for "USB device was unplugged!" message?
We have tried with different PCs, it works fine with some PC with "Windows 7"
but not with "Windows Vista".
Please let me know if there are any troubleshooting tips on this.
Best Regards
Kummi