This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP432P401R: Programming External MSP432 with on board XDS110, connection issues and cannot reset to factory settings

Part Number: MSP432P401R

Tool/software: Code Composer Studio

Hi all,

I'm working on my senior project for Computer Engineering and am trying to use the launchpad's XDS110 to program a MSP432 on a breadboard.  The breadboard has the necessary bypass caps that I have read about and according to the schematic. These being the one's in DC DC, analog VCC, and digital VCC. I also have the corresponding 5 programming signals going to the correct pins on the MSP. I also have the 91k resistor for DCOR.

I have been running into an error -613 where the debugger cannot connect to the MSP. Most forums on E2E suggest to do a factory reset if this is the case. In doing so, and following the instructions found at this URL 'http://www.ti.com/lit/ug/slau575g/slau575g.pdf' on page 29, but I can't perform a factory reset because of the following error: 

As you can see I can connect to the DAP core as instructed in the link provided, but when attempting to flash the MSP with the factory defaults I obtain this error 1170. The forums I've seen on this error say to do a factory reset: 

MSP432 Launchpad Error connecting to the target: Error -1170 - MSP low-power microcontroller forum -...

e2e.ti.com
Other Parts Discussed in Thread: ENERGYTRACE Hi All, I was debugging all day without a problem, and all the sudden, I changed a large section of the code, and
So I am in a never ending loop and am reaching out to you guys so I can hopefully get some help on how to further debug and program my external MSP432.

Thanks, James

**Attention** This is a public forum