Hai TI,
application: sensor: I need such a sensor which can detect non magnetic and magnetic metal(iron) and a sensor should produce a RAYS which penetrate thought the surface like wood and other surface and detect the object. laser light: when the sensor detect the object the controller should trigger the laser light and the light should fall on the object. controller: when the sensor detect the object the controller should trigger and send the signal to the laser light
I want metal detect sensor, Is there any wireless protocols will support.