This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P401R
Hello,
I want to interface ADS1243 with MSP432P401R processor.ADS1243 is run @4.9152MHz external crystal.ADC work on 3.3V supply. Vref+ is +2.5V and Vref- is 0V(GND). If input voltage given to ADC is 1V then what should be the output data code??( output data code=Vin/(Vref/2^n-1)=666666H is right or wrong??)
I am using default condition in register setup except speed bit and range bit is set to 1.SPI is working on 750kHz frequency.
Please check my code attached below and code sequence.
Thank you! When you start up a new thread be sure to use the part number (GPN) the question pertains to , in this case the "ADS1243" so it gets automatically posted to the correct forum.
I will close this thread in the MSP forum.
**Attention** This is a public forum