Part Number: MSP432P401R
Other Parts Discussed in Thread: ADS1292, ADS1292R
I am uploading my MSP432 code with which I am expecting to communicate to ADS1292(A board from proto-central is being used for the purpose) schematic is pc_ads1292r_brk_v3.pdf
I have tried my best in writing the code where I try to enable SPI, UART one by one with the help of SDK of MSP432 provided by TI, glad that it has helped me in writing fastly
but I find the problem in accessing the registers of AD1292 over SPI through MSP432, every time i read the board through SPI in debug mode each step takes lot of dealy than required
Here is my complete code bundle in the form of 6175.project.zip,
if you face any file not found during compilation , its due to include path , you have open Build>variables and change the MSP lib path to the where msp lib headers are present, or one has to download them if not there
Let me show the code flow
important decalrations / pins to which UART and SPI are connected
* Use with SPI Slave Data Echo code example.
*
* MSP432P401
* -----------------
* | |
* | |
* | |
* | P1.6|-> Data Out (UCB0SIMO)
* | |
* | P1.7|<- Data In (UCB0SOMI)
* | |
* | P1.5|-> Serial Clock Out (UCB0CLK)
* Author: Timothy Logan
*******************************************************************************/
#define ADS1292_DRDY_PORT GPIO_PORT_P2
#define ADS1292_DRDY_PIN GPIO_PIN3 //J4.34
#define ADS1292_CS_PORT GPIO_PORT_P5
#define ADS1292_CS_PIN GPIO_PIN1 //J4.33
#define ADS1292_START_PORT GPIO_PORT_P3
#define ADS1292_START_PIN GPIO_PIN5 //J4.32
#define ADS1292_PWDN_PORT GPIO_PORT_P3
#define ADS1292_PWDN_PIN GPIO_PIN7 //J4.31
/* SPI Master Configuration Parameter */
const eUSCI_SPI_MasterConfig spiMasterConfig =
{
EUSCI_B_SPI_CLOCKSOURCE_SMCLK, // SMCLK Clock Source
//3000000, // SMCLK = DCO = 3MHZ
1000000, // SMCLK = DCO = 1MHZ
500000, // SPICLK = 500khz
EUSCI_B_SPI_MSB_FIRST, // MSB First
EUSCI_B_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT, // Phase
EUSCI_B_SPI_CLOCKPOLARITY_INACTIVITY_HIGH, // High polarity
EUSCI_B_SPI_3PIN // 3Wire SPI Mode
};
/* UART Configuration Parameter. These are the configuration parameters to
* make the eUSCI A UART module to operate with a 115200 baud rate. These
* values were calculated using the online calculator that TI provides
* at:
* software-dl.ti.com/.../index.html
*/
const eUSCI_UART_Config uartConfig =
{
EUSCI_A_UART_CLOCKSOURCE_SMCLK, // SMCLK Clock Source
13, // BRDIV = 13
0, // UCxBRF = 0
37, // UCxBRS = 37
EUSCI_A_UART_NO_PARITY, // No Parity
EUSCI_A_UART_MSB_FIRST, // MSB First
EUSCI_A_UART_ONE_STOP_BIT, // One stop bit
EUSCI_A_UART_MODE, // UART mode
EUSCI_A_UART_OVERSAMPLING_BAUDRATE_GENERATION // Oversampling
};
please note these are code snippets only full code is present with project uploaded
Initialization part
int Setup_Initialization()
{
/* Halting WDT */
WDT_A_holdTimer();
/* Initialize the data ready and chip select pins*/
GPIO_setAsInputPin(ADS1292_DRDY_PORT,ADS1292_DRDY_PIN);
GPIO_setAsOutputPin(ADS1292_CS_PORT,ADS1292_CS_PIN);
GPIO_setAsOutputPin(ADS1292_START_PORT,ADS1292_START_PIN);
GPIO_setAsOutputPin(ADS1292_PWDN_PORT,ADS1292_PWDN_PIN);
/* Selecting P1.5 P1.6 and P1.7 in SPI mode */
GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P1,
GPIO_PIN5 | GPIO_PIN6 | GPIO_PIN7, GPIO_PRIMARY_MODULE_FUNCTION);
/* Configuring SPI in 3wire master mode */
SPI_initMaster(EUSCI_B0_BASE, &spiMasterConfig);
/* Enable SPI module */
SPI_enableModule(EUSCI_B0_BASE);
/* Enabling interrupts */
SPI_enableInterrupt(EUSCI_B0_BASE, EUSCI_B_SPI_RECEIVE_INTERRUPT);
Interrupt_enableInterrupt(INT_EUSCIB0);
Interrupt_enableSleepOnIsrExit();
/* Selecting P1.2 and P1.3 in UART mode and P1.0 as output (LED) */
GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P1,
GPIO_PIN2 | GPIO_PIN3, GPIO_PRIMARY_MODULE_FUNCTION);
GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN0);
GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
/* Setting DCO to 24MHz (upping Vcore) */
FlashCtl_setWaitState(FLASH_BANK0, 2);
FlashCtl_setWaitState(FLASH_BANK1, 2);
PCM_setCoreVoltageLevel(PCM_VCORE1);
CS_setDCOCenteredFrequency(CS_DCO_FREQUENCY_24);
/* Configuring UART Module */
UART_initModule(EUSCI_A0_BASE, &uartConfig);
/* Enable UART module */
UART_enableModule(EUSCI_A0_BASE);
/* Enabling interrupts */
UART_enableInterrupt(EUSCI_A0_BASE, EUSCI_A_UART_RECEIVE_INTERRUPT);
Interrupt_enableInterrupt(INT_EUSCIA0);
Interrupt_enableSleepOnIsrExit();
/*ADS 1292 Initialization*/
/*ADS1292 Reset*/
GPIO_setOutputHighOnPin(ADS1292_PWDN_PORT, ADS1292_PWDN_PIN);
delay(100); // Wait 100 mSec
GPIO_setOutputLowOnPin(ADS1292_PWDN_PORT, ADS1292_PWDN_PIN);
delay(100);
GPIO_setOutputHighOnPin(ADS1292_PWDN_PORT, ADS1292_PWDN_PIN);
delay(100);
/*Disable Start*/
GPIO_setOutputLowOnPin(ADS1292_START_PORT,ADS1292_START_PIN);
delay(20);
/*Enable Start*/
GPIO_setOutputHighOnPin(ADS1292_START_PORT,ADS1292_START_PIN);
delay(20);
/*Hard Stop*/
GPIO_setOutputLowOnPin(ADS1292_START_PORT,ADS1292_START_PIN);
delay(100);
/*Send Command Data START*/
ads1292_SPI_Command_Data(START);
/*Soft Stop*/
ads1292_SPI_Command_Data(STOP);
delay(50);
/*Stop read data continuous*/
ads1292_SPI_Command_Data(SDATAC);
delay(300);
ads1292_Reg_Write(ADS1292_REG_CONFIG1, 0x00); //Set sampling rate to 125 SPS
delay(10);
ads1292_Reg_Write(ADS1292_REG_CONFIG2, 0b10100000); //Lead-off comp off, test signal disabled
delay(10);
ads1292_Reg_Write(ADS1292_REG_LOFF, 0b00010000); //Lead-off defaults
delay(10);
ads1292_Reg_Write(ADS1292_REG_CH1SET, 0b01000000); //Ch 1 enabled, gain 6, connected to electrode in
delay(10);
ads1292_Reg_Write(ADS1292_REG_CH2SET, 0b01100000); //Ch 2 enabled, gain 6, connected to electrode in
delay(10);
ads1292_Reg_Write(ADS1292_REG_RLDSENS, 0b00101100); //RLD settings: fmod/16, RLD enabled, RLD inputs from Ch2 only
delay(10);
ads1292_Reg_Write(ADS1292_REG_LOFFSENS, 0x00); //LOFF settings: all disabled
delay(10);
//Skip register 8, LOFF Settings default
ads1292_Reg_Write(ADS1292_REG_RESP1, 0b11110010); //Respiration: MOD/DEMOD turned only, phase 0
delay(10);
ads1292_Reg_Write(ADS1292_REG_RESP2, 0b00000011); //Respiration: Calib OFF, respiration freq defaults
delay(10);
/*Stop read data continuous*/
ads1292_SPI_Command_Data(RDATAC);
delay(10);
/*Enable Start*/
GPIO_setOutputHighOnPin(ADS1292_START_PORT,ADS1292_START_PIN);
delay(20);
return 0;
}
communication with ADS1292
void ads1292_SPI_Command_Data(uint8_t command)
{
TXData = command;
GPIO_setOutputLowOnPin(ADS1292_CS_PORT, ADS1292_CS_PIN);
delay(2);
GPIO_setOutputHighOnPin(ADS1292_CS_PORT, ADS1292_CS_PIN);
delay(2);
GPIO_setOutputLowOnPin(ADS1292_CS_PORT,ADS1292_CS_PIN);
delay(2);
/* Polling to see if the TX buffer is ready */
while (!(SPI_getInterruptStatus(EUSCI_B0_BASE,EUSCI_B_SPI_TRANSMIT_INTERRUPT)));
/* Transmitting data to slave */
SPI_transmitData(EUSCI_B0_BASE, TXData);
GPIO_setOutputHighOnPin(ADS1292_CS_PORT, ADS1292_CS_PIN);
delay(2);
}
void ads1292_Reg_Write(uint8_t READ_WRITE_ADDRESS,uint8_t DATA)
{
uint8_t dataToSend;
switch (READ_WRITE_ADDRESS)
{
case 1:
DATA = DATA & (uint8_t)0x87;
break;
case 2:
DATA = DATA & (uint8_t)0xFB;
DATA |= 0x80;
break;
case 3:
DATA = DATA & (uint8_t)0xFD;
DATA |= 0x10;
break;
case 7:
DATA = DATA & (uint8_t)0x3F;
break;
case 8:
DATA = DATA & (uint8_t)0x5F;
break;
case 9:
DATA |= 0x02;
break;
case 10:
DATA = DATA & 0x87;
DATA |= 0x01;
break;
case 11:
DATA = DATA & 0x0F;
break;
default:
break;
}
// now combine the register address and the command into one byte:
dataToSend = READ_WRITE_ADDRESS | WREG;
GPIO_setOutputLowOnPin(ADS1292_CS_PORT, ADS1292_CS_PIN);
delay(2);
GPIO_setOutputHighOnPin(ADS1292_CS_PORT, ADS1292_CS_PIN);
delay(2);
GPIO_setOutputLowOnPin(ADS1292_CS_PORT,ADS1292_CS_PIN);
delay(2);
/*Send Register Location*/
/* Polling to see if the TX buffer is ready */
while (!(SPI_getInterruptStatus(EUSCI_B0_BASE,EUSCI_B_SPI_TRANSMIT_INTERRUPT)));
/* Transmitting data to slave */
SPI_transmitData(EUSCI_B0_BASE, dataToSend);
/*Number of Register to Write*/
/* Polling to see if the TX buffer is ready */
while (!(SPI_getInterruptStatus(EUSCI_B0_BASE,EUSCI_B_SPI_TRANSMIT_INTERRUPT)));
/* Transmitting data to slave */
SPI_transmitData(EUSCI_B0_BASE, 0x00);
/*Number of Register to Write*/
/* Polling to see if the TX buffer is ready */
while (!(SPI_getInterruptStatus(EUSCI_B0_BASE,EUSCI_B_SPI_TRANSMIT_INTERRUPT)));
/* Transmitting data to slave */
SPI_transmitData(EUSCI_B0_BASE, DATA);
delay(2);
GPIO_setOutputHighOnPin(ADS1292_CS_PORT, ADS1292_CS_PIN);
delay(2);
}
most important and problematic code is this
void delay( const int msec)
{
volatile int i;
for( i=0;i<msec;i++);
// __delay_cycles(msec);
}
main loop to send recieved data over UART
int main(void)
{
int i, j;
Setup_Initialization();
while(1)
{
if (ads1292dataReceived == true)
{
j=0;
for(i=0;i<6;i+=3) // data outputs is (24 status bits + 24 bits Respiration data + 24 bits ECG data)
{
uecgtemp = (unsigned long) ( ((unsigned long)SPI_RX_Buff[i+3] << 16) | ( (unsigned long) SPI_RX_Buff[i+4] << 8) | (unsigned long) SPI_RX_Buff[i+5]);
uecgtemp = (unsigned long) (uecgtemp << 8);
secgtemp = (signed long) (uecgtemp);
secgtemp = (signed long) (secgtemp >> 8);
s32DaqVals[j++]=secgtemp;
}
DataPacketHeader[0] = CES_CMDIF_PKT_START_1 ; // Packet header1 :0x0A
DataPacketHeader[1] = CES_CMDIF_PKT_START_2; // Packet header2 :0xFA
DataPacketHeader[2] = (uint8_t) (data_len); // data length
DataPacketHeader[3] = (uint8_t) (data_len>>8);
DataPacketHeader[4] = CES_CMDIF_TYPE_DATA; // packet type: 0x02 -data 0x01 -commmand
DataPacketHeader[5] = s32DaqVals[1]; // 4 bytes ECG data
DataPacketHeader[6] = s32DaqVals[1]>>8;
DataPacketHeader[7] = s32DaqVals[1]>>16;
DataPacketHeader[8] = s32DaqVals[1]>>24;
DataPacketHeader[9] = s32DaqVals[0]; // 4 bytes Respiration data
DataPacketHeader[10] = s32DaqVals[0]>>8;
DataPacketHeader[11] = s32DaqVals[0]>>16;
DataPacketHeader[12] = s32DaqVals[0]>>24;
DataPacketHeader[13] = CES_CMDIF_TYPE_DATA; // Packet footer1:0x00
DataPacketHeader[14] = CES_CMDIF_PKT_STOP ; // Packet footer2:0x0B
for(i=0; i<15; i++){
UART_transmitData(EUSCI_A0_BASE, DataPacketHeader[i]); // transmit the data over USB
}
ads1292dataReceived = false;
SPI_RX_Buff_Count = 0;
}
}
// PCM_gotoLPM0();
// __no_operation();
}
SPI Interrupt Handler
//******************************************************************************
//
//This is the EUSCI_B0 interrupt vector service routine.
//
//******************************************************************************
void EUSCIB0_IRQHandler(void)
{
uint32_t status = SPI_getEnabledInterruptStatus(EUSCI_B0_BASE);
volatile uint32_t jj;
SPI_clearInterruptFlag(EUSCI_B0_BASE, status);
if(status & EUSCI_B_SPI_RECEIVE_INTERRUPT)
{
RXData = SPI_receiveData(EUSCI_B0_BASE);
SPI_RX_Buff[SPI_RX_Buff_Count++] = RXData; // store the result data in array
if (SPI_RX_Buff_Count > 8){
SPI_RX_Buff_Count = 0;
ads1292dataReceived = true;
}
/* Delay between transmissions for slave to process information */
for(jj=0;jj<50;jj++);
}
}