This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP-EXP430G2
Tool/software: Code Composer Studio
I just got a MSP-EXP430G2 LaunchPad and tried to run the demo application (internal temperature measurement).
The code compiles and, as expected, the demo starts with blinking LEDs, and pushing the button starts temperature measurement, with red/green LED lighting up if the temperature rises/fall. However, the temperature data is supposed to be also transmitted via UART but I don't seem to receive anything.
I first tried to launch the GUI that comes with the demo, but at first I had an error messsge "Can't find file javaw.exe", so I downloaded Java. In a way it worked: I don't get an error message anymore, as strictly nothing happens when I try to launch the GUI.
After this, I downloaded Hyperterminal as most people found online seem to use it. When I plug the MSP, the port COM3 appears (it is the only available COM port anyway), so I started the communication with it with parameters 9600/8/1/N/N. I received nothing. I changed a few parameters (baud rate to 2400 or 4800, flow control XON/XOFF) with no effects.
I did not give up and tried to use PuTTY instead, with no more success. I should also mention that each time I tried with the TXD/RXD jumpers in vertical position, then in horizontal position.
I can't figure out what I am doing wrong....
Hello Henri,
Thank you for your detailed post. In the MSP-EXP430G2 LaunchPad Evaluation Kit User's Guide, I found where this demo application requires the serial communication port on the PC to be configured with 2400 bps, one stop bit, and no flow control to display the values correctly.
Here are some other resources that may be helpful as you continue debugging the issue.
temperature GUI not working for me - MSP low-power microcontroller forum - MSP low-power microcontrollers...
Need help with LaunchPad Tempurature Demo GUI - MSP low-power microcontroller forum - MSP low-power microcontrollers...
Regards,
James
MSP Customer Applications
Hello,
Henri Montjoie said:Moreover, today I tried a really simple piece of code a friend of mine wrote that just writes back in Tx what comes into Rx and got nothing either. That is, using my laptop, because using his, it did work. So the problem seems to be specific to my computer. I uninstalled the "usbser.sys" driver, it reinstalled automatically when I plugged back the LaunchPad and made no difference.
Excellent debugging! It does sound like it's an issue related to your PC. Could you try AdrianFer's instructions from this thread?
Let's try to figure this out together! I'll go ahead and list off the steps that I follow to get the GUI to work on my PC.
- Install the latest version of CCS or IAR - this will ensure the latest LaunchPad drivers are installed in your PC.
- As OCY mentioned, we do not need to have CCS or IAR open to run the GUI, simply to install the drivers
- Once the drivers are installed, we can plug in our LaunchPad via USB
- Navigate to your Device Manager to see which COM port your LaunchPad is connected to.
- Next, download and extract the GUI that Dung provided in a previous reply:
- Now you can run the GUI's windows executable file
- The GUI will display the connected COM ports, one of which is the COM port that our LaunchPad is connected to.
- Type in the index number that the LaunchPad is of your list - it typically is the last item.
- Then press [ENTER]
- Now, the GUI is waiting for data from the LaunchPad. To start reading temperature data and sending data to your PC, press switch P1.3
- At this point, the GUI should start displaying your instantaneous temperature.
Hope this helps! A lot of the times, people forget to press P1.3 to leave the "standby LED toggle" mode and enter the "temperature sensing" mode to start communicating with a PC.
Regards,
James
MSP Customer Applications
Hello again,
I disabled Avast, reinstalled CCS and Java and downloaded the provided GUI. Nothing happens when I try to open it. In the Task Manager I can see javaw.exe is running, but nothing happens.
Checking the dates, the GUI provided online is from 2014 so maybe I should downgrade Java to the 2014 version. But I am afraid the GUI not launching and not receiving anything when trying with PuTTY/hyperterminal are two different issues.
Thank you for your help, and if I find a solution I will post it.
Henri
**Attention** This is a public forum