Part Number: MSP432P401R
Other Parts Discussed in Thread: MSP-FET
Hi there,
Three MSP432P401R Development kit (two red board, one black board) has been purchased. out of three boards two of them heating up instantly after plugging the USB cable. (particularly MSP432p401R Chip).
1. Is it a problem, I am using MSP-FETflash Emulation tool with MSP-FET-432ADPTR (Rev 1.0) to flash the code.
2. I have configured the P4.5 as ADC and connected to one of the sensor analog output. For a duration time, I get expected voltage on this configured ADC pin(P4.5).
After some time, it was observed that voltage is always hanging around 3.0V to 3.1V on P4.5 (with respect to ground pin), Even after removing the sensor analog output from P4.5.
3.Another port pin(P4.0) has been configured for sensor analog output and now I am getting expected voltage continuously. But the problem is P4.5 hanging around 3.0V to 3.1V and MSP432p401R chip heating up with in a fraction of time.
Same situation with another Black development kit, but here P4.0 and P6.1 hanging around 3.0V to 3.1V.
These two are recent purchased boards. I have two older Development kits also, with same heating issue.
I had planned to use these boards for "water monitoring system" and code is working even after heating up. But this heating issue may cause a problem after real time deployment.
Please help me to overcome this issue, so that i can use these boards for my project.
Thanks,
Ajit