Other Parts Discussed in Thread: MSP430WARE, MSP430FR5994
Dear all,
I just started developing for the MSP430FR5994 µC using the evaluation board and the MSP430Ware. I want to get SPI communication working to test it out so I connected an oscilloscope to the UCB1 interface (P5.2 for clock and P5.0 for MOSI). I modified the example code in eusci_a_spi to work with eusci_b instead. However, I see nothing. The code looks like:
#include <msp430.h> #include "driverlib.h" //! Tested on MSP430FR5969 //! ----------------- //! /|\ | | //! | | | //! Master---+->|RST | //! | | //! | P2.0|-> Data Out (UCA0SIMO) //! | | //! | P2.1|<- Data In (UCA0SOMI) //! | | //! | P1.5|-> Serial Clock Out (UCA0CLK) //! //! This example uses the following peripherals and I/O signals. You must //! review these and change as needed for your own board: //! - SPI peripheral //! - GPIO Port peripheral (for SPI pins) //! - UCA0SIMO //! - UCA0SOMI //! - UCA0CLK //! //! This example uses the following interrupt handlers. To use this example //! in your own application you must add these interrupt handlers to your //! vector table. //! - USCI_A0_VECTOR //! //***************************************************************************** uint8_t RXData =0; uint8_t TXData = 0; void main(void) { volatile uint16_t i; WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer //Set P1.0 as an output pin. /* * Select Port 1 * Set Pin 0 as output */ GPIO_setAsOutputPin( GPIO_PORT_P1, GPIO_PIN0 ); //Set P1.0 as Output Low. /* * Select Port 1 * Set Pin 0 to output Low. */ GPIO_setOutputLowOnPin( GPIO_PORT_P1, GPIO_PIN0 ); // Configure Pins for LFXIN //Set PJ.4 and PJ.5 as Primary Module Function Input. /* * Select Port J * Set Pin 4, 5 to input Primary Module Function, (LFXIN). */ GPIO_setAsPeripheralModuleFunctionInputPin( GPIO_PORT_PJ, GPIO_PIN4 + GPIO_PIN5, GPIO_PRIMARY_MODULE_FUNCTION ); //Set external frequency for XT1 CS_setExternalClockSource(32768,0); //Set DCO frequency to max DCO setting CS_setDCOFreq(CS_DCORSEL_0,CS_DCOFSEL_3); //Select XT1 as the clock source for ACLK with no frequency divider CS_initClockSignal(CS_ACLK,CS_LFXTCLK_SELECT,CS_CLOCK_DIVIDER_1); //Start XT1 with no time out CS_turnOnLFXT(CS_LFXT_DRIVE_0); // Configure SPI pins // Configure Pins for UCA0CLK //Set P1.5 as Secondary Module Function Input. /* * Select Port 1 * Set Pin 5 to input Secondary Module Function, (UCA0CLK). */ GPIO_setAsPeripheralModuleFunctionInputPin( GPIO_PORT_P1, GPIO_PIN5, GPIO_SECONDARY_MODULE_FUNCTION ); // Configure Pins for UCA0TXD/UCA0SIMO, UCA0RXD/UCA0SOMI //Set P2.0, P2.1 as Secondary Module Function Input. /* * Select Port 2 * Set Pin 0, 1 to input Secondary Module Function, (UCA0TXD/UCA0SIMO, UCA0RXD/UCA0SOMI). */ GPIO_setAsPeripheralModuleFunctionInputPin( GPIO_PORT_P2, GPIO_PIN0 + GPIO_PIN1, GPIO_SECONDARY_MODULE_FUNCTION ); /* * Disable the GPIO power-on default high-impedance mode to activate * previously configured port settings */ PMM_unlockLPM5(); //Initialize Master EUSCI_B_SPI_initMasterParam param = {0}; param.selectClockSource = EUSCI_B_SPI_CLOCKSOURCE_ACLK; param.clockSourceFrequency = CS_getACLK(); param.desiredSpiClock = 500000; param.msbFirst = EUSCI_B_SPI_MSB_FIRST; param.clockPhase = EUSCI_B_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT; param.clockPolarity = EUSCI_B_SPI_CLOCKPOLARITY_INACTIVITY_HIGH; param.spiMode = EUSCI_B_SPI_3PIN; EUSCI_B_SPI_initMaster(EUSCI_B1_BASE, ¶m); //Enable SPI module EUSCI_B_SPI_enable(EUSCI_B1_BASE); //Clear receive interrupt flag EUSCI_B_SPI_clearInterrupt(EUSCI_B1_BASE, EUSCI_B_SPI_RECEIVE_INTERRUPT ); // Enable USCI_A0 RX interrupt EUSCI_B_SPI_enableInterrupt(EUSCI_B1_BASE, EUSCI_B_SPI_RECEIVE_INTERRUPT); //Wait for slave to initialize __delay_cycles(100); TXData = 0x1; // Holds TX data P1DIR |= 0x01; // Set P1.0 to output direction, blink function for debug P6DIR |= 0x04; // Set P6.2 to output direction, for debug //USCI_A0 TX buffer ready? while(1) { while (!EUSCI_B_SPI_getInterruptStatus(EUSCI_B1_BASE, EUSCI_B_SPI_TRANSMIT_INTERRUPT)) ; //Transmit Data to slave EUSCI_B_SPI_transmitData(EUSCI_B1_BASE, TXData); i = 10000; // SW Delay do i--; while(i != 0); P1OUT ^= 0x01; // Toggle P1.0 using exclusive-OR P6OUT ^= 0x04; // Toggle P6.2 using exclusive-OR } __bis_SR_register(LPM0_bits + GIE); // CPU off, enable interrupts __no_operation(); // Remain in LPM0 } #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector=USCI_A0_VECTOR __interrupt #elif defined(__GNUC__) __attribute__((interrupt(USCI_A0_VECTOR))) #endif void USCI_A0_ISR (void) { switch (__even_in_range(UCA0IV,4)){ //Vector 2 - RXIFG case 2: //USCI_A0 TX buffer ready? while (!EUSCI_A_SPI_getInterruptStatus(EUSCI_A0_BASE, EUSCI_A_SPI_TRANSMIT_INTERRUPT)) ; RXData = EUSCI_A_SPI_receiveData(EUSCI_A0_BASE); //Increment data TXData++; //Send next value EUSCI_A_SPI_transmitData(EUSCI_A0_BASE, TXData ); //Delay between transmissions for slave to process information __delay_cycles(40); break; default: break; } }
The only additional modification from the original code is that I added blinking to the LED as a debug thing.