This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-THREEPHASEMETER-F67641: TIDM-THREEPHASEMETER-F67641

Part Number: TIDM-THREEPHASEMETER-F67641
Other Parts Discussed in Thread: MSP430F67641, TIDA-00601, TIDA-01094, TIDA-01088

Hi, 

I am looking to confirm if the above part works with a non invasive CT sensor as well as the invasive system.?

  • Hello,

    Are you asking if the MSP430F67641 works with isolated and non-isolated current sensors? If so, yes it will work with shunts (non-isolated) or CTs (isolated) but the connections may be different. Also, the EVM may not have been designed to use shunts. There's an isolated RS-232 interface that protects your PC.

    I would recommend looking at the following TI Designs: TIDA-00601, TIDA-01088, TIDA-01094

    Regards,

    James

    MSP Customer Applications

**Attention** This is a public forum