This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EZ430-CHRONOS: eZ430-chronos-868

Part Number: EZ430-CHRONOS

My husband wants to use the eZ430-chronos-868 as a referee watch at korfball matches.

The standard Chronos has yet to be expanded with the 12wiki referral software Photo Service The watch has 5 buttons.

Specific software for korfball competitions (and other sports) has been set up to keep track of time.

The makers of this software sold the watch initially via korfbalhorloge.nl but have stopped since a while.

The software is now overcoded.

The above information can be found on www.scheidsrechtershorloge.com I downloaded a User Guide via www.ti.com/chronoswiki.

On page 14 of the manual you will find that - if you have a Windows computer - you have to download SLAC341. I have done that. Then the RF Access Point (the supplied white usb) is plugged into the usb port.

On page 15 the explanation starts on how the watch should be configured.

But as soon as I start, I get the error message you see in the second attachment. However, I did not remove the USB.

 

I have tried several things.

Software reinstalled and from two other computers.

But I keep getting the same error message.

The most important is:

How do I install everything via the computer (because now it does not seem to connect).

And how do I get to that referee software for korfball and how do I install it?

I hope you can help me further.

Thanks in advance.

**Attention** This is a public forum