Part Number: MSP432P401R
Other Parts Discussed in Thread: DAC8311
Hello,
I want to transfer some data from RAM to one of the SPI interfaces, which is connected to a DAC.
The DAC expects 16 bits without de-asserting the CS line in between. Currently I generate the CS line manually with a GPIO pin.
To speed up the whole process, I want to use a DMA transfer.
My question (before starting to dig into the DMA documentation in more depth):
- Is is possible to transfer 16 bit words (2 byte sequence) to a SPI interface with DMA and automatically create the correct CS signal (asserted/de-asserted before/after a 2-byte transfer)?
- Could I use a second DMA channel to generate the CS signal?
Any hint and help is very welcome!
BR, Andreas