This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/MSP430F6723: F6723

Part Number: MSP430F6723

Tool/software: WEBENCH® Design Tools

Hello:

     F6723 is used to make products,the power supply is 0.5F 6V Fala capacitor, which is depressed by LDO to 3.3V for MCU.Now, when I do the EDS test, we find that the product is dead,redondload the program or short connect the reset  pin can not return to normal;Another phenomenon is that when using the hand to hold the board, it will also appear.

     The capacitance can only be discharged to normal operation.

     Why does this happen? Is there anything to do with Fala's capacitive power supply? How to deal with it..Thanks.