This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E401Y: How to configure static IP addresses. MSP432E401y launchpad

Part Number: MSP432E401Y

In a related thread, someone asked how to configure static ip addresses using the NDK

The following answer was given

****
In the udpecho.c there is a file called ndk_tirtos.c which configures the stack

In the initIP function you would need to add a new Cfg for CFGTAG_CLIENT where you can configure the static IP allocation

for more details please refer to the C:/ti/simplelink_msp432e4_sdk_2_10_00_17/docs/ndk/NDK_API_Reference.html in the SDK under section 4.3.5

****

The person who started the thread was looking for a snippet of example code which was not provided.  I looked into these references above and did not find them as helpful as I would have liked.  All of the examples in the SDK seem to use DHCP.  I have had a hard time finding an example of InitIP for static IP address configuration.  In one of the manuals, there is a nice example of InitIP given for DHCP.  I would much appreciate it if someone could provide an example of InitIP for static ip configuration. 

**Attention** This is a public forum