Hi Folks,
we've been using the MSP430F5437 for a couple of years in a hand held device that is equipped with an ethanol fuel cell sensor. Years ago we choose that MCU because it had a rather large flash memory and a good 12 bit ADC and many, many I/O ports for different peripherals.
Now we plan to to make a very reduced version of that device, downsizing this to a real minimum version without display and other stuff.
So we basically need a smaller brother of that MCU. Small in size, only a few I/Os, UArt, I2C, 2 timers are enough.
The signal from the ethanol fuel cell detector is a rather slow DC signal. So no special speed requirements.
Ethanol signal is channel 2
Probably most available MSP could do that, but essential to our measurement is an exact (stable) AD-Conversion,
with a stable internal voltage reference and a stable internal time reference over a wide temperature range.
Currently we use 12bit ADC. Most of smaller MCUs have only 10bit ADC.
Since we calibrate the sensor with a reference gas and get a reference curve, stable reproducibility i(over time and temperature) s more important than absolute accuracy.
I'd like to stay within the MSP430 family to be able to reuse the JTAG flasher and IAR Workbench License for MSP430.
Is there any MCU you would recommend?
Thanks in advance!
HB