This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
GPN: MSP430F5418A
Problems customer encounter:
1. Can the bootloader upgrade the code with the flash address after 0x10000?
Flash Address allocation:
bootloader:0x5c00-0x6bff
APP:0x6c00-0xfdff 0x10000-0x16000
It is not possible to erase and write the 0x10000-0x16000 part when upgrading the APP area with the bootloader. If the code of the APP area is reduced to be within the range of 0x6c00-0xfdff, it can be erased correctly and the APP area code can be successfully written to the flash through the serial port.
2. If the bootloader method does not work, is there any other way to upgrade the microcontroller program through the serial port?
Best Regards,
Rock Su
**Attention** This is a public forum