This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5324: ACLK and SMCLK shifted to DCO during Noise.

Part Number: MSP430F5324

Hi

i am using MSP430F5324 in my projects. it has 25Mhz , XT2 crystal. problem is that whenever i bring my Phone (in calling mode) near to my Device, some time it is getting hanged or shifted to DCO (1Mhz , Default) .

if i use 25Mhz DCO instead of XT2 Crystal . it works fine. 

Could you please help me to know what would be the root cause for this,

Thanks in Advance

Regards

Deepak 

  • Deepak,
    I think your phone will disturb the crystal maybe due to improper layout of the PCB and you see how the fail safe detection is triggered due to a XT2 fault. In this case the automatic fail-safe operatio is triggered and the clock system switch back to DCO. This is described in users guide chapter 5.2.12 UCS Module Fail-Safe Operation:

    The crystal oscillator fault bits XT1LFOFFG, XT1HFOFFG, and XT2OFFG are set if the corresponding
    crystal oscillator is turned on and not operating properly. After the fault bits are set, they remain set until
    reset in software, even if the fault condition no longer exists. If the user clears the fault bits and the fault
    condition still exists, the fault bits are automatically set, otherwise they remain cleared.

    If a fault is detected for the oscillator sourcing MCLK, MCLK is automatically switched to the DCO for its
    clock source (DCOCLKDIV) for all clock sources except XT1 LF mode. If MCLK is sourced from XT1 in LF
    mode, an oscillator fault causes MCLK to be automatically switched to the REFO for its clock source
    (REFOCLK). This does not change the SELM bit settings. This condition must be handled by user
    software.

    So please implement fault handling of the OFIFG and the XT2OFFG to switch back to XT2 after the crystal recovered from external noise.
    Also please consider the oscillator layout guides described in following Apps Note, it refers to 32 kHz but is true for HF crystals as well.
    http://www.ti.com/lit/slaa322

**Attention** This is a public forum