This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5324: Getting incorrect output frequency using ACLK

Part Number: MSP430F5324


Hello there,

In our project we are using the ACLK digitally out. We use 38KHz crystal for ACLK and using the following code to specify the ACLK,

 

            BIS.B   #BIT0,&P1DIR            ; ACLK set out to pins

            BIS.B   #BIT0,&P1SEL            ;

 

            BIS    #XT2OFF,UCSCTL6;                       // Set XT2 Off

            BIC    #XT1OFF,UCSCTL6;                       // Set XT1 On

            BIS    #XCAP_3,UCSCTL6;                       // choose the load cap

            BIS.B  #BIT4+BIT5,&P5SEL;                     // Port select XT1

 

When we probe the P1.0 by a logic analyzer we measure 32KHz (like the trimmed low-frequency oscillator (REFO),​) rather than 38KHz. Can you help us understand what we may be doing wrong to get the incorrect frequency out?

Thanks,

-Amanda

**Attention** This is a public forum