Part Number: MSP430F1611
I am using MSP430F1611, and I want to perform SPI communication between MSP430F1611(Master) and FPGA(Slave), I can send data successfully from MSP430F1611 to FPGA and get miso data in U0RXBUF and RXBUF0, now problem is how to store data from ( U0RXBUF and RXBUF0) in any other variable, please help me to solve this problem.
Thanks
Regard.
Code:
#include <msp430.h>
char MST_Data = 0x4F;
unsigned char msd,msd1,msd2;
unsigned int j;
unsigned int i;
int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
P3DIR =0x001;
P3SEL = 0x00E; // Setup P3 for SPI mode
// U0CTL = (0x0070u) /* USART 0 Control */
// CHAR = (0x10) /* Data 0:7-bits / 1:8-bits */
// SYNC = (0x04) /* UART / SPI mode */
// MM = (0x02) /* Master Mode off/on */
U0CTL = CHAR + SYNC + MM + SWRST; // 8-bit, SPI, Master
U0TCTL = CKPH + SSEL1 + STC; // Polarity, SMCLK, 3-wire
// U0BR0 = (0x0074u) /* USART 0 Baud Rate 0 */
// U0BR0 = 0x064; // SPICLK = SMCLK/2
// U0BR1 = (0x0075u) /* USART 0 Baud Rate 1 */
U0BR1 = 0x000;
// UMCTL0 = U0MCTL /* USART 0 Modulation Control */ reg name
U0MCTL = 0x000;
// ME1 = (0x0004u) /* Module Enable 1 */
ME1 = USPIE0; // Module enable
U0CTL &= ~SWRST; // SPI enable
IE1 |= URXIE0; // Recieve interrupt enable
__enable_interrupt(); // Enable interrupts
//TXBUF0 = 0x00;
msd = RXBUF0;
msd1 = U0RXBUF;
i = 50000; // Delay
do (i--);
while (i != 0);
msd = RXBUF0;
msd1 = U0RXBUF;
{msd = RXBUF0;
msd1 = U0RXBUF;
TXBUF0 = MST_Data; // Transmit first character
LPM0; // CPU off
}
msd = RXBUF0;
msd1 = U0RXBUF;
} // End Main
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USART0RX_VECTOR
__interrupt void SPI0_rx (void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USART0RX_VECTOR))) SPI0_rx (void)
#else
#error Compiler not supported!
#endif
{
j = 5000; // Delay
do (j--);
while (j != 0);
TXBUF0 = MST_Data;
/*
j = 10000; // Delay
do (j--);
while (j != 0);
TXBUF0 =0x34;
j = 10000; // Delay
do (j--);
while (j != 0);
TXBUF0 =0x56;
j = 10000; // Delay
do (j--);
while (j != 0);
TXBUF0 =0x78;
j = 10000; // Delay
do (j--);
while (j != 0);
TXBUF0 =0x9A;
*/
//TXBUF0 =0xab;
// TXBUF0 =0xbb;
//P3OUT =0x00;
}