This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have just purchased a new MSP-Gang programmer, that is being used to program 8 MSP430FR5994 at the same time.
The programmer has been set up and run in interactive and standalone. For an hour the unit worked perfectly and it programmed all the boards.
However after a while it was unreliable and would randomly fail to work giving various errors when running even on boards it had already passed.
It has no consistency in its function, to check we put a scope on the pcb while we did an erase check and instead of getting a steady square wave we got anything but.
The self test says no errors in the unit, it is being powered with a 9v 2250mA psu and vcc is pin 2, we are SBC and using pins 1,2,7 and 9 only
I have made a cable that is only 60mm long and it still randomly fails to pass a board.
The errors will be random on the same pcb everytime, error 23, error 33, error 58. then the pcb will pass several times and then it will randomly fail.
If i place a new pcb on the tester it will pass a few times and then the same thing.
If i use a single MSP-FET programmer the pcb's pass every single time with no failures and on repeated runs on each pcb.
Could there possibly be an issue with the unit?
Thanks
Hi Matt unfortunately I have neither the target board or launchpad, however i can put in a request to purchase one of them today as it would be interesting to see what happens.
I spent yesterday running the pcb's again first putting new blank pcb's on the programmers and all working first time, i then hit "go" again and only a couple would re-program again, hit "go" again and sometimes none, sometimes one or two.
As the unit is primarily flashing blank boards of the production line and has no issues there it will be used for now however, I will try and get another unit in this week and run that to see if that has the same issue or not.
I will keep the thread open for now and update you as soon as possible
Regards
Simon
**Attention** This is a public forum