This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I'm doing an Ethernet communication test with the DP83849IVS-EVK board.
I want to modify the register for changing to LED mode 3
I have "MSP-EXP430G2ET" LAUNCH PAD
I read "usb-2-mdio software tool" (SNLU 197)
BUT This document is a little different "MSP-EXP430G2ET"
[QUESTION]
Which pin on the "MSP-EXP4300G2ET" board should I connect the MDIO / MDC pins of the DP83849IVS-EVK board?
Could you tell me?
Thanks
from Donell
Hi Winter Yu
Thank you for reply
and as you know
I am trying to run USB-2-MDIO using the MSP-EXP430G2E2 Launchpad and the DP83849IVS-EVK board.
but I have problems with PHY searching still.
My conditions is
1) Connected
: DP83849IVS-EVK MDIO/ J1 Pin2 ---- MSP-EXP430G2E2 board MDIO / P1.5
DP83849IVS-EVK MDC/ J1 Pin5 ---- MSP-EXP430G2E2 board MDC / P1.4
and GND PIN connected
2) On the MSP-EXP430G2E2 board
: the drivers are installed
: successfully flasehd, down to Launchpad and LED1 and LED2 of fully illuminated
( file: usb_2_mdio_G2.HEX)
3) On the DP83849IVS-EVK board
: J36 (PHYAD1) and J37(PHYAD2) => strapped high or open
4) On USB-2-MDIO
: PORT can be opened, port status reads "HW connected"
However , when I run the "File -> find PHY ID" , all 32 PHY IDs show "NOI Available"
Could you tell me any idea or what problem?
Hi Winter
Thank you for your reply
I checked step7 ,
Port Status window display "green" and "HW Connected" on "USB-2-MDIO" program
Is there any possibility that the port can not be connected even under the above conditions?
Donell
**Attention** This is a public forum