Tool/software: Code Composer Studio
Hi,
A strange problem was found. The MSP430F248 chip for a product was connected with 2M crystal oscillator. During operation, the program would turn off the crystal oscillator and enter the low power mode, waking up the crystal oscillator every 1s.
In the test, it was found that the crystal oscillator of several products could not be activated, and the reset signal given by the external watchdog every 30 seconds did not work. The voltage of passive crystal oscillator at both ends was about 1V, and there was no waveform. If the power is turned on after the power is cut off, it can be restored to normal.
Questions:
1. When will crystal vibration fail to start? Many products have been produced (1000), only a few examples.
2. How to judge whether the crystal oscillator is out of order or whether the microcontroller can not reset and initialize?
3. When the MCU receive a reset signal, will it give the crystal oscillator an excitation signal?
Thank you very much!!!
Kevin