This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Hi,
I am having an issue with CCS Version: 9.0.1.00004. The project keeps failing when trying to import FRAM-utilities on the MSP430FR5739.
This is only happening on Linux Ubuntu 18.04. I have tried windows, and the problem does not exist. I have tried a different workspace, different project as well to import from resource explorer.
The same error keeps showing up. Any workaround to fix this?
See the screenshot for the error.
[E0300] The following symbols are undefined: gmake: *** [fram-utilities/ctpl/ctpl_low_level.obj] Error 1 gmake: Target 'all' not remade because of errors.
**Attention** This is a public forum