This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P401R
Tool/software: TI-RTOS
I'm using the TI-RTOS example from the resource explorer on the Launchpad. The RTOS is up and running. Now I'm trying to modify the ACLK using
MAP_CS_initClockSignal(CS_ACLK, CS_REFOCLK_SELECT, CS_CLOCK_DIVIDER_2);
in the main function and with this config, the tick count is off by a factor of two (Task_sleep(500) takes twice as long) . Which tells me that the tick counter has decided to source off the ACLK and the default divider for ACLK must have been 1.
What is the proper way to adjust the ACLK so that the built in tick count gets adjusted?
Hello,
I have tried to use the ClockFreqs_setFrequency and the Clock_tickReconfig APIs without success. I do not believe there is a mechanism to update the clock frequency for the MSP432. The default configuration for the tick is to use TIMER_A0 in continuous mode being sourced from ACLK. What are you trying to accomplish? Would it be possible to setup another clock object to achieve the desired timing without adjusting ACLK?
Regards,
Chris
I'm trying to change the ACLK to a lower frequency for another use in my project. But doing so has a side effect of making the timeouts for many of the RTOS functions wrong (i.e. sleep(500) is no longer a 500 tick delay, its 1000 ticks, mailbox_pend(x,y,20) is no longer a 20 tick delay).
I guess the only solution is to set the tick count value in the RTOS too 500usec so when I drop the ACLK, the tick count will be 1000usec. But its a sloppy solution and I was hoping for more. Does everyone just use the default ACLK value?
Hello,
An alternative would be to change the performance level, which includes the clock settings. The intent of this discussion was to demonstrate power consumption but can also be used to manipulate the ACLK.
Regards,
Chris
I am going to close this. Please use 'Ask a related question' for further inquiries.
Regards,
Chris
**Attention** This is a public forum