Part Number: MSP-FET430UIF
Other Parts Discussed in Thread: MSP-FET
Tool/software: Code Composer Studio
I bought MSP-FET430UIF, Rev.2.0.6.
When I connect the emulator with my computer, multiple errors occur.
First, it says "Error Initializing Emulator" and asks me to update the emulator.
Even after the update,
"No USB FET was found", "Could not set device Vcc", "The voltage 1167 value is not connect/allowed for the USB FET", "Interface Communication error", "MSP-FET430UIF already in use"
comes up each time.
I tried to solve this problem based on your previous solutions to similar questions, opening the emulator and connect J5.
However, there is no J5, available to connect in this the most recent version of the board.
Here I attached the image of errors and image of the board.
I did all my best to sol
ve this problem but none of them are working.
Please help me. I need to use this emulator ASAP.