This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5887: After power off and restart, sampling disorder

Part Number: MSP430FR5887


Dear all:

        I used MSP430FR5887 to design the magnet-free sensor. When my program was just written, I ran sample OK.But then the power went off and the sampling went haywire.

The power supply is 3V, I use the voltage regulator to supply 3V, and this is also the case after the power failure and restart.
What's the reason, please?It doesn't seem to be a hardware problem. Is there something wrong with my software?

Thank you!

  • Hello Timsen,

    Thanks for your post. One of our team members will be looking into your post and replying shortly.

    Regards,

    James

  • Hi, Timsen, 

    I want to double check with you about the failed case: When you power on and programming with sample code, the board worked well. But immediately, the 3v power dropped and the FR5887 restart. Then the power dropped again and MCU restart again. Right? 

    What is the code example? What is the peripheral you used in the code example and what is the external circuit driving by MCU? If no external circuit connected to MCU and the only simple code examples run such as the "msp430fr69xx_1.c", will the failed case occur? 

    From the datasheet, the MCU will reset when 3v power drop to VSVSH- (1.75v~1.85v). Do you have tested the how much drop for the power supply for the failed case? We need to find the components which consume big current so as to cause the 3v power dropped. 

    Thanks, 

    Lixin 

  • Hi Timsen,

    if you do a sensor design I assume you have a voltage signal connected to any GPIO pin right?

    Did you check that during power down all GPIOs were powered off as well? Otherwise you might have supplied your device via ESD diodes of the GPIO which can cause malfunctions. This is a hot topic especially if you're using an LDO which might not be able to sink power.

    There are some people who do not consider this in a right way therefore I wrote an Apps Note some time ago: Feel free to check if this might cause your problem:
    www.ti.com/lit/an/slaa689/slaa689.pdf

**Attention** This is a public forum