This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
//User need to switch on the motor with half-covered matal disc to finish the calibration
Set_DAC();
Is there any requirement for the speed of the dial to calibrate the DAC when the dial rotates? If so, what is the speed.
Hi,
yes there are limits based on the scan rate that is determined by the SW. For the regular SW that comes with the EVM I had good results with 2-4 rotations/sec.
**Attention** This is a public forum