This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F47177: MSP430F47177 MSPBoot – Main Memory Bootloader for MSP430™ Flash Microcontroller SLAA600D Code Reset Problem

Part Number: MSP430F47177

Tool/software: Code Composer Studio

Dear Sir,

We want to add bootloader facility in our product that requires single image bootloader facility using UART.

As we have found some reference for the same by application note of  SLAA600D.
.
And we make some changes in the lnk_msp430f47177.cmd according to our uC MSP430F47177. 

Our problem with the code is it doesn't reset the code and go to main() during Debug mode.

Please suggest the changes in the below code attach if any we also attach the file folder for the same.5707.bootloader_MSP430F47177.zip

/* ============================================================================ */
/* Copyright (c) 2014, Texas Instruments Incorporated                           */
/*  All rights reserved.                                                        */
/*                                                                              */
/*  Redistribution and use in source and binary forms, with or without          */
/*  modification, are permitted provided that the following conditions          */
/*  are met:                                                                    */
/*                                                                              */
/*  *  Redistributions of source code must retain the above copyright           */
/*     notice, this list of conditions and the following disclaimer.            */
/*                                                                              */
/*  *  Redistributions in binary form must reproduce the above copyright        */
/*     notice, this list of conditions and the following disclaimer in the      */
/*     documentation and/or other materials provided with the distribution.     */
/*                                                                              */
/*  *  Neither the name of Texas Instruments Incorporated nor the names of      */
/*     its contributors may be used to endorse or promote products derived      */
/*     from this software without specific prior written permission.            */
/*                                                                              */
/*  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" */
/*  AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,       */
/*  THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR      */
/*  PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR            */
/*  CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,       */
/*  EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,         */
/*  PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; */
/*  OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,    */
/*  WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR     */
/*  OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,              */
/*  EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.                          */
/* ============================================================================ */

/******************************************************************************/
/* lnk_msp430f47177.cmd - LINKER COMMAND FILE FOR LINKING MSP430F47177 PROGRAMS     */
/*                                                                            */
/*   Usage:  lnk430 <obj files...>    -o <out file> -m <map file> lnk.cmd     */
/*           cl430  <src files...> -z -o <out file> -m <map file> lnk.cmd     */
/*                                                                            */
/*----------------------------------------------------------------------------*/
/* These linker options are for command line linking only.  For IDE linking,  */
/* you should set your linker options in Project Properties                   */
/* -c                                               LINK USING C CONVENTIONS  */
/* -stack  0x0100                                   SOFTWARE STACK SIZE       */
/* -heap   0x0100                                   HEAP AREA SIZE            */
/*                                                                            */
/*----------------------------------------------------------------------------*/
/* Version: 1.127                                                             */
/*----------------------------------------------------------------------------*/

/****************************************************************************/
/* SPECIFY THE SYSTEM MEMORY MAP                                            */
/****************************************************************************/
/* RAM Memory Addresses */
__RAM_Start = 0x1100;                 /* RAM Start */
__RAM_End = 0x30FF;                     /* RAM End */
    /* RAM shared between App and Bootloader, must be reserved */
    PassWd = 0x1100;                 /* Password sent by App to force boot  mode */
    StatCtrl = 0x1102;             /* Status and Control  byte used by Comm */
    CI_State_Machine = 0x1103;         /*  State machine variable used by Comm */
    CI_Callback_ptr = 0x1104;   /* Pointer to Comm callback structure */
    /* Unreserved RAM used for Bootloader or App purposes */
    _NonReserved_RAM_Start = 0x1108; /* Non-reserved RAM */

/* Flash memory addresses */
__Flash_Start = 0x3100;             /* Start of Application area */
   /* Reserved Flash locations for Bootloader Area */
    __Boot_Start = 0xF800;         /* Boot flash */
    __Boot_Reset = 0xFFFE;                          /* Boot reset vector */
    __Boot_VectorTable = 0xFFC0;      /* Boot vector table */
    __Boot_SharedCallbacks_Len = 6; /* Length of shared callbacks (2 calls =4B(msp430) or 8B(msp430x) */
    __Boot_SharedCallbacks = 0xFFBA; /* Start of Shared callbacks */
     _BOOT_APPVECTOR = __Boot_SharedCallbacks;       /* Definition for application table             */
    _Appl_Proxy_Vector_Start = 0xF702; /* Proxy interrupt table */
    /* Reserved Flash locations for Application Area */
MEMORY
{
    SFR                     : origin = 0x0000, length = 0x0010
    PERIPHERALS_8BIT        : origin = 0x0010, length = 0x00F0
    PERIPHERALS_16BIT       : origin = 0x0100, length = 0x0100
    // RAM from _NonReserved_RAM_Start - __RAM_End
    RAM                     : origin = 0x1108, length = 0x1FF8
    USBRAM                  : origin = 0x0200, length = 0x800
	// Info Mem Sections
	INFOA                   : origin = 0x10C0, length = 0x40
    INFOB                   : origin = 0x1080, length = 0x40
    INFOC                   : origin = 0x1040, length = 0x40
    INFOD                   : origin = 0x1000, length = 0x40
    // Flash from _App_Start -> (APP_PROXY_VECTORS-1)
    FLASH                   : origin = 0x3102, length = 0xC600
    FLASH2                  : origin = 0x10000, length = 0xA000
    // Interrupt Proxy table from  _App_Proxy_Vector_Start->(RESET-1)
    APP_PROXY_VECTORS       : origin = 0xF702, length = 252
    // App reset from _App_Reset_Vector
    RESET                   : origin = 0xF7FE, length = 0x0002
}

/****************************************************************************/
/* SPECIFY THE SECTIONS ALLOCATION INTO MEMORY                              */
/****************************************************************************/

SECTIONS
{
    .bss        : {} > RAM                /* GLOBAL & STATIC VARS              */
    .data       : {} > RAM                /* GLOBAL & STATIC VARS              */
    .sysmem     : {} > RAM                /* DYNAMIC MEMORY ALLOCATION AREA    */
    .stack      : {} > RAM (HIGH)         /* SOFTWARE SYSTEM STACK             */

    .text:_isr  : {}  > FLASH            /* Code ISRs                         */
    #ifndef __LARGE_CODE_MODEL__
        .text       : {} >> FLASH               /* CODE                 */
    #else
        .text       : {} >> FLASH | FLASH2      /* CODE                 */
    #endif

        .cinit      : {} > FLASH        /* INITIALIZATION TABLES*/
    #ifndef __LARGE_DATA_MODEL__
        .const      : {} >> FLASH       /* CONSTANT DATA        */
    #else
        .const      : {} >> FLASH2 | FLASH    /* CONSTANT DATA        */
    #endif

    .cio        : {} > RAM                /* C I/O BUFFER                      */

	.infoA     : {} > INFOA              /* MSP430 INFO FLASH Memory segments */
    .infoB     : {} > INFOB
    .infoC     : {} > INFOC
    .infoD     : {} > INFOD

    .APP_PROXY_VECTORS : {} > APP_PROXY_VECTORS /* INTERRUPT PROXY TABLE            */
   /* .int00       : {}               > INT00
    .int01       : {}               > INT01
    .int02       : {}               > INT02
    .int03       : {}               > INT03
    .int04       : {}               > INT04
    .int05       : {}               > INT05
    .int06       : {}               > INT06
    .int07       : {}               > INT07
    .int08       : {}               > INT08
    .int09       : {}               > INT09
    .int10       : {}               > INT10
    .int11       : {}               > INT11
    .int12       : {}               > INT12
    .int13       : {}               > INT13
    .int14       : {}               > INT14
    DMA          : { * ( .int15 ) } > INT15 type = VECT_INIT
    BASICTIMER   : { * ( .int16 ) } > INT16 type = VECT_INIT
    PORT2        : { * ( .int17 ) } > INT17 type = VECT_INIT
    USCIAB1TX    : { * ( .int18 ) } > INT18 type = VECT_INIT
    USCIAB1RX    : { * ( .int19 ) } > INT19 type = VECT_INIT
    PORT1        : { * ( .int20 ) } > INT20 type = VECT_INIT
    TIMERA1      : { * ( .int21 ) } > INT21 type = VECT_INIT
    TIMERA0      : { * ( .int22 ) } > INT22 type = VECT_INIT
    SD16A        : { * ( .int23 ) } > INT23 type = VECT_INIT
    USCIAB0TX    : { * ( .int24 ) } > INT24 type = VECT_INIT
    USCIAB0RX    : { * ( .int25 ) } > INT25 type = VECT_INIT
    WDT          : { * ( .int26 ) } > INT26 type = VECT_INIT
    COMPARATORA   : { * ( .int27 ) } > INT27 type = VECT_INIT
    TIMERB1      : { * ( .int28 ) } > INT28 type = VECT_INIT
    TIMERB0      : { * ( .int29 ) } > INT29 type = VECT_INIT
    NMI          : { * ( .int30 ) } > INT30 type = VECT_INIT*/
    .reset       : {}               > RESET  /* MSP430 RESET VECTOR         */ 
}

/****************************************************************************/
/* INCLUDE PERIPHERALS MEMORY MAP                                           */
/****************************************************************************/

-l msp430f47177.cmd

**Attention** This is a public forum