This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5728: Low temperature out of spec usage

Part Number: MSP430FR5728

I am investigating using an MSP430FR type device with a small package at very low temperatures. The FRAM is of particular interest. I found that the MSP430FR5728 will continue running when it is submerged in LN, -196C, but then fails to run after powering down and back up again. The programmer gives me the error "Error connecting to the target: Device configuration data inconsistent. Please discontinue using/replace target device". From the error, it seems that maybe the configuration is somehow corrupted? I have tested another MSP430  non FRAM device at these temperatures without any apparent issues.

I understand that the parts are not rated for these temperatures.

**Attention** This is a public forum