This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We have recently begun production of a new device based on an MSP430 microcontroller. We are using an MSP-FET and MSP Flasher to program the devices.
Our production staff programmed approximately 50 devices earlier this week. Today, I received a report that it wasn't working. I exchanged the MSP-FET device, and this solved the problem. I'm now testing the problematic MSP-FET on my development PC, and it's not working here either.
I use this command line:
MSP430Flasher.exe -w MyProgram.hex -v -g -z [VCC]
It pauses for an unusually long time at "Setting VCC to 3000 mV", then reports "Exit: 44", "ERROR: Could not set device Vcc".
At this time, we sometimes also receive a Windows error message: "One of the USB devices attached to this computer has malfunctioned, and Windows does not recognize it."
We were previously using MSP Flasher 1.3.15. I upgraded to version 1.3.20 today, and allowed it to upgrade the firmware on our MSP-FET devices. This did not make any difference that I could see.
Can you offer any advice? Thanks.
Hi Graham,
Have you tried the recovery (Cold Boot) process mentioned in the MSP Debuggers user's guide (section 5.6.5.3)? Can you try using it both with CCS and MSP Flasher after doing the recovery process?
Regards,
Luis R
Hi Graham,
CCS is not needed, but it's more of a recommendation to check if the issue persists using both tools.
Regards,
Luis R
Hi Luis,
The photo on page 20 of SLAU647M.pdf does not quite match the appearance of my MSP-FET.
Is the reset jumper location now called J2? I'd have to solder two pins to the board, which is no problem, except that I won't likely have time today. I'd also like to know that doing so won't void whatever warranty is applicable here.
-- Graham
That's correct, please try with J2.
The procedure is suggested by the User's Guide, so it won't void warranty.
Please keep us updated
LR
Hi Graham,
I'm glad to hear that your MSP-FET is working again.
I noticed that my FET takes a couple of seconds setting VCC the first time I plug it in, but then it's faster if I reprogram again.
Regards,
Luis R
**Attention** This is a public forum