This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P401R
Tool/software: Code Composer Studio
Hello,
I would like to use ADC14 inside the MSP432P401R launchpad to measure the wind sensor in very low sampling rate. (<10Hz)
Is it necessary to use voltage follower and anti-aliasing filter?
The output impedance of the sensor is approximately 50~150 ohm.
PS. where can I find the input impedance of ADC14 of MSP432P401R.
Regards,
YHH
Hi,
I think you can use a simple RC circuit as an AA filter in front of the ADC input.
For input impedance see this:
https://e2e.ti.com/support/microcontrollers/msp430/f/166/t/626119
Thanks
**Attention** This is a public forum