Current software versions:
Gas Demo Application UltrasonicGasFR6043_02_20_00_12
USSSWLib USS-02_20_00_19
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Evgeny,
I am reaching out to one of our USS experts who will provide more information soon.
Thanks,
Mitch
Hi Evgeny,
The minimum excitation frequency possible with this device is 133kHz. In order to get to these lower excitation frequencies, the project must be recompiled with a PLL setting of 68MHz(instead of 80). The GUI doesn't support request updates with configurations at these lower excitation frequencies so you can only view captures and waveform data after recompiling an image with this lower frequency excitation.
BR,
Leo
**Attention** This is a public forum