Greetings,
Can I use in MSP430F2619S-HT Timer module to generate PWM for BLDC motor control ( I would need 6 outputs for 3x PWM_H and PWM_L drivers)
Thank you in advance,
Gadi Fishel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Greetings,
Can I use in MSP430F2619S-HT Timer module to generate PWM for BLDC motor control ( I would need 6 outputs for 3x PWM_H and PWM_L drivers)
Thank you in advance,
Gadi Fishel
Hello Gadi,
I'm would say, probably. The Timer B has 7 capture compare registers. Usually the first register is used for generating the PWM period and then the others can be used to generate outputs and all the Timer B outputs are brough out on the P4.x pins. As long as all 6 outputs can run on the same PWM period/time scale then I think you should be okay with actually generating the signals.
The Timer B is discussed in detail in Chapter 13 of the User's Guide: https://www.ti.com/lit/ug/slau144j/slau144j.pdf
I would read through that chapter and make sure it'll meet all your needs.
Thanks,
JD
Hello JD,
Thank you so much for the advise.
I will check the option.
Sincerely,
Gadi Fishel
**Attention** This is a public forum