Part Number: MSP430F5419A
Hello,
My customer would like to add an external reset signal to F5419A.
At the same time the board needs a Spy-Bi-Wire debug capability.
Then I would think the circuit is good, but do you have any suggestions or concerns ?
My points are:
- The base is the SBW circuit in the SLAU278Y, p24.
- The external reset source should be open-collector or open-drain.
I copied the external reset source circuit from MSP-EXP430F5529: