This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: MCU device initialization failed - MSP-GANG

Expert 6470 points
Part Number: MSP432P401R
Other Parts Discussed in Thread: MSP-GANG

We have an MSP432P401R-based PCB and have problems with reprogramming the MSP432.

We started writing firmware and used MSP-GANG Programmer to write the firwmare versions into the flash of the MSP432. So far it was successful, the GANG-Programmer always succeeded in erasing and writing the firmware. Today, after another firmware update (while trying out new features) it all stopped working. The Gang-Programmer is unable to find the MCU (it says: ERROR 23: MCU device initialization failed.)

On another PCB (same design), it works fine, so the last software update probably caused an error in the MCU and that is why it cannot communicate. 
In this case, should a factory reset be performed on the MSP432? How to do it?

I have attached a screenshot of the gang programmer. The settings have not been changed and with these settings I can communicate and overwrite the flash memory of hte other PCB's MSP432.

**Attention** This is a public forum