Other Parts Discussed in Thread: MSP430F6459
Customer feedback initially MSP-Gang programmer is able to program when running with small quantity. After 2 weeks of deployment, it shows Error 23: MCU device init. It is unable to perform programming...error message always show unable to init MCU.Customer used it to program MSP430F6459, connection through Vcc,Gnd Test and RST pin. Customer has performed a selftest on the device and found that RST signal on Cav 2 to 7 are having ERROR.The target MCU has R1(47K) and C1(1nF) at the RST pin of the target MCU on board.The programmer is already having ERROR on RST during selftest. The firmware version of the MSP-Gang is 01.02.08.00 . Please advice whether the MSP-Gang programmer is faulty. Thank you.