Other Parts Discussed in Thread: CAPTIVATE-PHONE
Hi team,
I am posting this inquiry on behalf of our customer. To make sure that I will not miss any information, I will paste here the customer inquiry:
"I need to use TI development kit (CAPTIVATE-FR2633) for tracking two or three capacitive sensors are in the same range of capacity as some of the ons TI placed on the demo board with sliders, proximiy and keyboard configuration (NBO000181 - on a paper label) and the design environment doesn't let me place two identical capacitors in the circuit. So, since I think that the system just cannot be that limited, I am certain that I am doing something wrong and I wonder if you have a solution for this particular job: just have generic capacitors hooked to some ports of an MSP430 micro and see how they do."
Here's the set up of the customer.
It’s just a couple of capacitors inserted into the 48-pin connector.
The customer would like to be able to demonstrate the functionality with moving the capacitors from port to port so that he could see how to accommodate various board configurations, basically with the same level of complexity but with the capacitors being connected at various pins.
Please let me know if there's anything you want to clarify with the customer.
Thanks!
Jonathan