This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
dear sir ,
here we are using MSP430F2418 , is it possible to enable the FOTA for the same ?
if not , please suggest the controller that may have FOTA feature , along with MSP430F2418 pin configuration.
Hi Mannem,
I assume you're talking about Firmware Over The Air updates?
To be able to update FW over the air you need RF communication features. Within the MSP430 portfolio only the CC430Fxxx devices are equipped with RF on chip, and in more detail, it is an equivalent radio to CC1101, means sub 1GHz.
The other option is to use an MSP430 in combination with an RF device. In this case you could use any MSP430 + an RF Transceiver from TI. This could be an RF only, like CC2500/CC1101, or a complete SoC, like CC13xx/CC26xx.
Best regards,
Peter
Yes , i am talking about Firmware Over The Air updates,
but i am going to use the GPRS 4G module instead of RF Transceivers.
please suggest the controller as per that.
Hi Mannem,
I am not sure what GPRS module you're talking about. Do you have a part number for me?
Best regards
Peter
Hi Mannem,
many thanks for the additional information. Unfortunately these are not parts from TI and it is not easy to see, which requirements the use of this parts would impose on the µC to enable the use of the respective modules. Thus, if you would like us to make proposals on a suitable MSP430, you need to deliver a list of features and parameters required, then I could help you with selecting the optimum MSP430 derivative.
Best regards
Peter
**Attention** This is a public forum