Hi,
My customer has a question about the internal reference voltage (VSD24REF) and sampling rate of SD24_B.
Could you tell us about the following?
1. Is the variation between the minimum value (1.151V) and the maximum value (1.174V) of the internal reference voltage (VSD24REF) due to temperature? Or individual differences?
2. Is the sampling rate setting range up to 2Msps?
In the thread below, it was stated as 2MHz.https://e2e.ti.com/support/microcontrollers/msp430/f/166/p/225131/792607
Best regards,
O.H