Hello TI Community,
Per the datasheet, abs max voltage to any pin is VCC+0.3V. While I realize that saturating an ADC input will not give an accurate value, will it cause damage or long term reliability issues? For example, suppose I'm using VCC=3.0V and VREF = 1.5V with an analog input that may go as high as 3.3V. I only care about when the ADC input falls below 1.5V (the non saturating condition), so as long as my measurement is accurate in that range that's all I care about. As I said though, the input could spend a fair amount of time sitting up to 3.3V max. Not my design and I don't have any leverage to change the input divider without supporting rationale that this is a problem.
Please let me know.
Thank you,
Chris